PDOs for AKD, AKD2G, AKD-N, S300, or S700
The KAS Motion Engine interacts with the AKD, AKD2G, AKD-N, S300, or S700 drives through CANopen objects in the selected PDOs.
- Some of the ML and MC function blocks require specific CANopen objects in the PDOs.
- Defaults:
- AKD, AKD2G, and AKD-N PDOs include all of the CANopen objects needed by the motion engine and function blocks.
- S300 and S700 PDOs include only the minimal CANopen objects required by the KAS motion engine.
PDO Types
- RxPDO — From Controller to Drive (RxPDO)
- TxPDO — From Drive to Controller (TxPDO)
Examples
These are examples where the PDO object is passed as an argument in the function block.
Example 1
MLSmpConECAT( PipeNetwork.SMP1, 1001, 16#2050, 0);
Where:
PipeNetwork.SMP1is a Sampler block ID.1001is the EtherCAT address for the first device.16#2050(0x2050) is the object index and0is the subindex for the AKD’s “Position actual value 2” object.
Example 2
MLCNVConnectEx(PipeNetwork.CNV1, PipeNetwork.AXIS1, EC_ADDITIVE_TORQUE_VALUE, 0 ) ;
The argument is a constant based on the object index.
Example 3
MLSmpConPNAxis(PipeNetwork.SMP1, PipeNetwork.AXIS1, ML_SECOND_FEEDBACK_POSITION);
Where:
ML_SECOND_FEEDBACK_POSITION specifies the secondary actual position from the Pipe Network Axis.
-
- The ML_SECOND_FEEDBACL_POSITION constant has been deprecated and only AKD devices supported it.
It is deprecated because the AKD2G supports more than one secondary feedback.